Running the Project

This chapter explains how to build, download and run your project.

The Device Toolbar

Step Description
1 Set the compilation options to run your project in Debug or Release modes, and choose if you want to activate the Online Changes
2 Compile the application and see all the remaining warnings and errors
3 Connect the KAS IDEClosed "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger to the target device
4 Download the Application compiled on the KAS IDE to the target device
5 Start / stop the device, and control your application with the script commands